Skip to main content
SRedd.5
Senior III
July 22, 2023
Solved

Systick time missing

  • July 22, 2023
  • 23 replies
  • 11911 views

I am running the motor control workbench B-G431B-ESC1 board. The systick fires at every 2K frequency as per the user manual and the waveform matches when i toggle, but the problem is sometimes it misses as shown

SRedd5_0-1689998582490.png

I want to debug and find out why it misses those timings in between. Please suggest how do i find out? I am also running CAN in parallel at 500KBPS.

    This topic has been closed for replies.
    Best answer by SRedd.5

    I modified the algorithm of CAN and behavior is ok now, i mean i transmit 3 messages at one time, after 1 sec another 3 messages with total of 12 messages

    1st sec -> 3messages

    2nd sec -> 3 messages

    3rd sec -> 3 messages

    4th sec -> 3 messages

    repeat like this.

    23 replies

    Johi
    Senior II
    July 22, 2023

    What is the effect of disabling CAN?

    SRedd.5
    SRedd.5Author
    Senior III
    July 24, 2023

    Sorry for late response yes it is because of CAN task, how do i solve the problem? I will try to reduce the code in CAN ISR and put it in while(1).

    Johi
    Senior II
    July 24, 2023

    No problem. Have you considered generating your waveform directly with a TIMER routed to GPIO or if the waveform is a bit more complex use DMA to drive GPIO and use a timer to drive the DMA timing? That way CAN ISR will not interfere with waveform generation. If needed I can provide an example code.

    Bob S
    Super User
    July 24, 2023

    DIsclaimer: I know nothing about the motor workbench code and run-time environment.

    That said, if your "systick" is the normal ARM/STM32 systick timer, it typically defaults to the lowest interrupt priority.  You can change that and make it a higher priority (lower numeric value) than then CAN interrupts.  Presuming of course that the CAN interrupts can tolerate some delay when the systick interrupts them.  Or use a different timer (with a higher interrupt priority than the CAN interrupt) for that purpose.

    Is the waveform you showed just "toggle a pin" inside the systick ISR to show when it is missed (or delayed), changing the priority may be all that is needed.  If that is indeed a waveform needed by your system, then changing to DMA/GPIO instead of code in an ISR as @Johi suggested might be needed.

    SRedd.5
    SRedd.5Author
    Senior III
    July 25, 2023

    My main concern is SysTick_Handler is missing timing in between. The code is as below.

    void SysTick_Handler(void)
    {
    #ifdef MC_HAL_IS_USED
    static uint8_t SystickDividerCounter = SYSTICK_DIVIDER;
      /* USER CODE BEGIN SysTick_IRQn 0 */
     
      /* USER CODE END SysTick_IRQn 0 */
      if (SystickDividerCounter == SYSTICK_DIVIDER)
      {
        HAL_IncTick();
        HAL_SYSTICK_IRQHandler();
        SystickDividerCounter = 0;
      }
      SystickDividerCounter ++;
    #endif /* MC_HAL_IS_USED */
     
      /* USER CODE BEGIN SysTick_IRQn 1 */
      /* USER CODE END SysTick_IRQn 1 */
        MC_RunMotorControlTasks();
    CAN_Task();
    HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_12);
     
       /* USER CODE BEGIN SysTick_IRQn 2 */
      /* USER CODE END SysTick_IRQn 2 */
    }
    How do i increase the priority of Systick interrupt? I am toggling the GPIO inside Systick handler.
    LCE
    Principal II
    July 25, 2023

    Search your files for "HAL_NVIC_SetPriority(SysTick_IRQn;" (might be in STM32xxx_hal.c)

    and set it to:

    HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);

    As BobS said: lower number, higher priority. So give some higher numbers to the other interrupts.

    Check the description before the declaration of HAL_NVIC_SetPriority.

    SRedd.5
    SRedd.5Author
    Senior III
    July 25, 2023

    When i searched this is what i found

    HAL_NVIC_SetPriority(SysTick_IRQn, uwTickPrio, 0U);

    #define __NVIC_PRIO_BITS 4U /*!< STM32G4XX uses 4 Bits for the Priority Levels */

    uint32_t uwTickPrio = (1UL << __NVIC_PRIO_BITS); /* Invalid PRIO */

    hence uwTickPrio  is 16, but as per the ST documentation

    @PAram PreemptPriority: The pre-emption priority for the IRQn channel.
    * This parameter can be a value between 0 and 15
    * A lower priority value indicates a higher priority

    The priority can be between 0 to 15 only.

     

     

    LCE
    Principal II
    July 25, 2023

    Simply set both priorities to 0.

    SRedd.5
    SRedd.5Author
    Senior III
    July 25, 2023

    It does not solve the problem still i get some missing times.

    SRedd.5
    SRedd.5Author
    Senior III
    July 25, 2023

    Ok i will update the code.

    LCE
    Principal II
    July 25, 2023

    What's happening if you turn of other interrupts, or at least do nothing (except setting a flag maybe) in the interrupt handlers?

    LCE
    Principal II
    July 25, 2023

    BTW, the skipped pulse on the scope looks quite regular, maybe you show the interrupt handler where you toggle the GPIO.

    And have you reduced the other interrupts' priorities?

    SRedd.5
    SRedd.5Author
    Senior III
    July 25, 2023

    I have shown the code in my 2nd post. I have put the CAN interrupt lowest but unfortunately I am using the Systick as the base time for CAN as well do I need to use other timer. There is huge code in CAN and transmitting lot of messages around 9 with periodicity of 1 sec.

    LCE
    Principal II
    July 25, 2023

    There's a lot happening in your SysTick_Handler, why that divider? 
    That makes me assume that you are using a very high SysTick frequency, which again means that this interrupt handler is called too often. It should be good enough with 1 kHz for most applications.

    And yes, try using another timer as base time for CAN.
    You are using it for timeouts, message scheduling or what?

    SRedd.5
    SRedd.5Author
    Senior III
    July 25, 2023

    Mainly for CAN message scheduling.

    LCE
    Principal II
    July 25, 2023

    And again:
    what's the time between the dropped pulses?
    Maybe that might tell you something.