STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1743 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4892 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9594 Views
  • 5 replies
  • 3 kudos

MCSDK Encoder Alignment

Hi.I m new at ST MCSDK and i was reading some documents about mcsdk position control until waiting for my custom board arrive. I have few questions about encoder mounting and alignment operation.According to the documant AN5464; it seems that for fin...

qqwq.1 by Associate II
  • 1640 Views
  • 0 replies
  • 0 kudos

motor control workbench

In the latest version of the STM32 Motor Control Workbench (6.2.1), I am unable to select hall sensor-based speed control for my STM32 Nucleo F030R8 board with the IHM08M1 driver. Despite selecting hall sensor in the motor specifications, the option ...

#iR by Associate II
  • 1644 Views
  • 2 replies
  • 1 kudos

Resolved! 6-step speed fluctuation & current spikes

I am facing issues while running a BLDC motor using the 6-step algorithm on the STEVAL-SPIN3201 board. The only modification I have made is to the Hall effect sensor low-pass filter to address noisy input signals.I am encountering the following probl...

scope_47.png 1500rpm_no_load.png

Resolved! STEVAL-ctm006V1 startup failure.

Hi,mcsdk: 6.2.1control board: nucleo-g474reBridge: XNUCLEO-IHM09M2Power Board: STEVAL-CTM009V1Motor: Motenergy ME1304 I prepared motor profile for ME1306 with help of EVSPIN32G4 and used in configuration,described above.But now I get Startup failure ...

tasifacij by Associate III
  • 4789 Views
  • 9 replies
  • 0 kudos

Resolved! Overcurrent protection hardware feature not showing

[VERSION]: 6.2.1[TOOL]: MC WB[DETAILS]:We are making a custom PCBA based on a STm32G474METx. Algorithm is FOC.I'm trying to activate Over current protection, but:My hwVariant is (parameters are not tuned/configured yet)"type": "SingleInput_RawCurrent...

LLang_0-1705396238928.png LLang_1-1705396572616.png
LLang by Associate
  • 2678 Views
  • 4 replies
  • 2 kudos

Space vector Modulation implementation

Hi GuysI have a question about space vector modulation implementation. I'm reading a code for ST MC workbench designed to run SVPWM. there is calculations for sector identification in space vector that I can't get it's idea completely. if someone ana...

photo9837570863.jpg photo9837570759.jpg

Resolved! Red flashing light when I connect my B-G431B-ESC1 board

Hi there, I recently purchased the B-G431B-ESC1 and when I connect it to my USB port, immediately a red flashing light appears. There are two other solid green lights. I am also not able to connect my ST-LINK to flash firmware, and this may be relate...

HudsonSam by Associate II
  • 11484 Views
  • 1 replies
  • 0 kudos