STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1730 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4875 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9575 Views
  • 5 replies
  • 3 kudos

Motor Power Calculation (Watt)

Hello, I am working on a motor control project that is to be driven battery-powered. This means that the DC current has to be monitored in order to avoid overloading the battery. I have made a Control Loop which takes in a DC Current reference as inp...

MC_STEVAL_FOC_5A_Current_Limit_v3.png {6248B94D-DE7D-40BE-9ED5-2D173B42E8C9}.png

NEW STM32 MC-SDK version 5.Y.4

Dear STM32 Motor Control community membersWe are very pleased to announce the new release 5.Y.4 of the XCUBE_MCSDK. This release fix the compatibility issue you may have faced with cubeMX 6.4.This release is the last planed of the 5 versions, and as ...

cedric H by ST Employee
  • 8681 Views
  • 10 replies
  • 4 kudos

STM32G431 Custom Control Board Noisy Current Sense

Hello. I have developed a custom control board utilizing similar architecture to that of the STM-B-G431B ESC board. I am experiencing difficulties trying to tune the PI coefficients for current Iq and Id. The output plot from the motor pilot looks re...

TS-LMG by Associate III
  • 1901 Views
  • 1 replies
  • 0 kudos

Resolved! Changing Slotted Motor Phase using SDK V5.4.8

I'm trying to control the AirFan MFA0290 BLOWER using the ST motor control SDK V5.4.8 and the generated pulses on the Phases and Halls are as pictured below (brown, red, orange ) (phase 1, phase 2, phase3) respectively but i need to make those pulses...

khaledsaeed_0-1711457889338.png khaledsaeed_1-1711458024976.png khaledsaeed_2-1711458103176.png

Resolved! External use of internal buck regulator of STSPIN32G4

Hello,I want to ask a question about internal buck switching converter of STSPIN32G4.We want to use its output voltage of 10V or 12V to supply an external potentiometer.Is this converter indicated to use for power supply external devices requiring 10...

Motor does not start

Tools:MCSDK - 6.2.1MC Workbench 6.2.1STM32CubeMX - 6.10STM32CubeIDE - 1.14.1ST Motor Pilot - 1.2.5Hardware SetupNucleo-0G474RESTEVAL-IPM30B (My own version of the board, same circuit and layout)X-NUCLEO-IHM09M2I-PMSM motor 9 Pole Pairs, 220W, 36VDETA...

Jorgie by Associate III
  • 2953 Views
  • 6 replies
  • 0 kudos