STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1816 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4956 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9713 Views
  • 5 replies
  • 3 kudos

NEW STM32 MC-SDK version 5.Y.4

Dear STM32 Motor Control community membersWe are very pleased to announce the new release 5.Y.4 of the XCUBE_MCSDK. This release fix the compatibility issue you may have faced with cubeMX 6.4.This release is the last planed of the 5 versions, and as ...

cedric H by ST Employee
  • 8959 Views
  • 10 replies
  • 4 kudos

STM32G431 Custom Control Board Noisy Current Sense

Hello. I have developed a custom control board utilizing similar architecture to that of the STM-B-G431B ESC board. I am experiencing difficulties trying to tune the PI coefficients for current Iq and Id. The output plot from the motor pilot looks re...

TS-LMG by Associate III
  • 1983 Views
  • 1 replies
  • 0 kudos

Resolved! Changing Slotted Motor Phase using SDK V5.4.8

I'm trying to control the AirFan MFA0290 BLOWER using the ST motor control SDK V5.4.8 and the generated pulses on the Phases and Halls are as pictured below (brown, red, orange ) (phase 1, phase 2, phase3) respectively but i need to make those pulses...

khaledsaeed_0-1711457889338.png khaledsaeed_1-1711458024976.png khaledsaeed_2-1711458103176.png

Resolved! External use of internal buck regulator of STSPIN32G4

Hello,I want to ask a question about internal buck switching converter of STSPIN32G4.We want to use its output voltage of 10V or 12V to supply an external potentiometer.Is this converter indicated to use for power supply external devices requiring 10...

Motor does not start

Tools:MCSDK - 6.2.1MC Workbench 6.2.1STM32CubeMX - 6.10STM32CubeIDE - 1.14.1ST Motor Pilot - 1.2.5Hardware SetupNucleo-0G474RESTEVAL-IPM30B (My own version of the board, same circuit and layout)X-NUCLEO-IHM09M2I-PMSM motor 9 Pole Pairs, 220W, 36VDETA...

Jorgie by Associate III
  • 3061 Views
  • 6 replies
  • 0 kudos

Resolved! Motor Profiler - Motor Won't Spin - (from MC Workbench 6.2.0)

Hi,This is my first post on the forum so my apologies if I’m doing something wrong.OS:Windows 10 64-bitSoftware:STM32CubeIDE 1.14.1Motor Control Workbench 6.2.0ST Motor Pilot v1.2.4Hardware:Dev Kit:                      P-NUCLEO-IHM002Control Board: ...

Resolved! Bug Report - ASPEP Protocol Ping Packets

Hello,I am currently trying to implement an ASPEC Controller in C# to communicate with a motor control dev board over the UART (essentially, creating motor pilot with the ability to modify as needed).  So far, I have implemented Beacon and ping packe...

ccut93 by Associate III
  • 4336 Views
  • 3 replies
  • 1 kudos

Resolved! Board not recognised by Motor Control SDK

Hello,I have tried multiple times to connect a Nucleo-G4R31B to the motor profiler.The software fails to recognise the boards at any of the preset baud rates.The board is recognised by the computer and is visible on the device manager. It is also pro...

akash_hegde_1-1712035354680.png akash_hegde_0-1712035215142.png akash_hegde_2-1712040239676.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.