User Activity

The V5 motor control workbench had an "UPDATE" button to update the ioc without losing user added changes. The current V6.1.0 workbench doesn't have the update button and always generates a new ioc file, losing all of my additions that took an hour ...
I have a project that was originally developed under Windows using the motor control workbench. Under Windows, I can successfully open, edit and re-compile the project IOC file (using the built-in Eclipse device configuration tool). I've transferre...
The "documentation" suggests that any IO port that can act as an interrupt is usable, but the motor control workbench only has selections for A2, A9 and B10, all of which are used for other peripherals. The document suggests selecting a "dummy" port...