STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1595 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4741 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9451 Views
  • 5 replies
  • 3 kudos

Resolved! Bug Report: Unimplemented Registers

Hardware: EVSPIN32G4-DUALConfiguration: 1-shunt FOC, Observer + PLL Bug location: register_interface.cRegisters in Question:FLUXWK_BUS_MEASMC_REG_PULSE_VALUE, MC_REG_BEMF_ZCRMC_REG_BEMF_UMC_REG_BEMF_VMC_REG_BEMF_WDescription:When these registers are ...

ccut93 by Associate III
  • 974 Views
  • 1 replies
  • 0 kudos

How to use motor without hall?

Issue in short: When changing to a motor without hall, the project breaks and doesn't build anymore. Full Explanation:I started a project that uses a motor with hall sensors.The project is set up in the MCWB to primarily use the Observer and as Auxil...

DMeie.2 by Senior II
  • 1925 Views
  • 2 replies
  • 1 kudos

Feature Request: BISS C encoder support

We have a project that requires high torque, low speed, precision control of axial flux motors (40+ poles). We use rotary absolute encoders that provide position over RS-422 BISS C protocol. It does not appear there is support for this type of setup ...

cpoole by Associate
  • 3509 Views
  • 1 replies
  • 0 kudos

Check PWM Duty Cycle on Motor Control

Hi.., Currently, I'm using STSPIN32F0601 and driving the BLDC motor using ST-MCSDK-5.4.5 and I'm very new to it. After spending a couple of weeks studying, I know how to call the API to check parameters like VBUS, Motor Speed, Motor Power, Phase curr...

Agga by Associate II
  • 3548 Views
  • 5 replies
  • 0 kudos

how to add project on STM32 IDE

Hi,I am following the instructions given in this page: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motorI have some question regarding that.1. Are these the right examples that are shown in the figure?ACIM-NUCLEOG431RB-IHM023...

NAYAN_0-1707481959561.png
NAYAN by Associate
  • 1407 Views
  • 1 replies
  • 0 kudos

dc stepper motor

I am attempting to control the speed of a DC stepper motor using an Infineon TLE8444SL motor driver. The four outputs of the driver are connected to the motor, with inputs 1 and 2 shorted and connected to pin Pa1, and inputs 3 and 4 shorted and conne...

NASOK.1 by Associate II
  • 1686 Views
  • 1 replies
  • 0 kudos

Resolved! Motor setting for B-G431B-ESC1

Hello eveybody.Before try to uss a motor with encoder drive by B-G431B-ESC1 board, need some setting ? Examples:Encoder A and B sequence respect to motor rotation CW or CCW ?Encoder phased to electrical motor phase ?Any Other ?

UniRob by Associate III
  • 3074 Views
  • 4 replies
  • 0 kudos