STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1725 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4873 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9560 Views
  • 5 replies
  • 3 kudos

Motor profiler and NUCLEO-G474RE (IHM16M1)

I plan to start using the MC SDK, and I was ready to get a Nucleo-G474RE with a IHM16M1.But when looking at the motor profiler utility, I noticed that the combination is not supported. There is support for the IHM16M1 and the STM32G474 processor in t...

ACarr.4 by Associate
  • 1915 Views
  • 2 replies
  • 0 kudos

Workbench connection failed

Hi all. Today our custom design board just arrive and we begin to test. Our custom board controllinng via STM32F103RBT6 product and programmed through the Stlink programmer using Stlink Utility software. We have a problem about connection using COM p...

qqwq.1 by Associate II
  • 2073 Views
  • 3 replies
  • 0 kudos

Resolved! About x-cube-mcsdk ver.6.2.1 and nucleo-h745zi

I set up x-cube-mcsdk least ver.6.2.1 workbench with a combination of nucleo-h745zi(motor control board) and x-nucleo-ihm08m1(motor inverter board).The pin configuration is the default setting.Where should I connect x-nucleo-ihm08 to nucleo-h745zi?

RIG by Associate III
  • 3015 Views
  • 4 replies
  • 2 kudos

about the charge boot capacitor time and duty

hi,    I set the charge boot capacitor time with 100ms and the duty with 50%. the picture is below, and I captured the waveform by the scope. low side (green,16V from drive circuit),high side (red, 3.3V from MCU). the low side boot time is 125us. why...

截屏2024-04-02 12.52.36.jpg 截屏2024-04-02 12.54.56.jpg

b-g431b-esc1 Overcurrent at the start

I have a custom motor controlled with the b-g431b-esc1 that I have been able to run in position control mode without overcurrent protection. As soon as I activate overcurrent protection the motor goes in the fault state when I click the "start" of th...

giova_ by Associate II
  • 1301 Views
  • 1 replies
  • 0 kudos

IHM14A1

Hello,I would try to use  the IHM14A1 shield  and  for now i only have a nucleo F2 series . it seemed in the document that this nucleo is not supported , can somebody tell me if it can't works  or maybe with some modifications on the example code. th...

Resolved! Motor Control Protocol Suite Library

Hi everybody,I was looking at the documentation for the MCSDK6 (great work btw), in particular to the Motor Control Protocol Suite section.Everything is well documented, however, I was wondering if is there any DLL available in order to facilitate th...

Resolved! dynamically changing Timer ARR and CCR1

Hi everyone,I am currently working on controlling a stepper motor using a PWM signal. I want to dynamically update the speed of the motor using different ARR and CCR1 values. Controlling the stepper works fine until an uncertain amount of time when t...

Smar by Associate II
  • 3199 Views
  • 2 replies
  • 1 kudos

ST Board with inline phase current (AN5423)

Hello. I am just starting in the world of motor control with ST parts and SW, so please be patient with me.I have checked different motor control boards for BLDC, and some related documentation, and I found special interesting the AN5423.https://www....

PCota by Associate
  • 1874 Views
  • 1 replies
  • 0 kudos