STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1726 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4875 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9572 Views
  • 5 replies
  • 3 kudos

Resolved! Excessive current on startup - Rev-up setting is ignored

[Basic Info]We're currently having issues with our custom board.It is based on the G431RB in FOC and 3-Shunt mode, with a DRV8323RS as the gate drive and for amplifying and attenuating the current measurement.The motor is a low-inductance (8.1µH) hig...

DMeie.2 by Senior II
  • 2522 Views
  • 2 replies
  • 1 kudos

Resolved! How to invert current reading?

For our motor control project we're using a driver IC with integrated opamp stage intended for current measurement.This opamp stage inverts the current reading compared to the Current sensing signals conditioning model, see here:To correct the curren...

grafik.png
DMeie.2 by Senior II
  • 3488 Views
  • 6 replies
  • 2 kudos

MDSK5.4.8 CAN Communication Not working

hi.I using MDSK 5.4.8 with NUCLEO F103RB / NUCLEO IMH07M1The speed control operation was confirmed through the variable volume.So now, I want to operate CAN 2.0A CommunicationI already set CUBEMX pin & CAN setting.Now, i just send message(tx test) De...

chocho by Associate II
  • 2242 Views
  • 1 replies
  • 0 kudos

Motor speed issues B-G431B-ESC1

Hi!Trying to use a Leopard LC2830-980KV motor with the B-G431B-ESC1. I have managed to program the device with the MC Workbench and can run the motor using the Motor Pilot software. However I can't seem to get the speed over 2100 rpm for some reason....

Skärmklipp3.PNG Skärmklipp4.PNG Skärmklipp2.PNG

Resolved! PWM input problem with B-G431B-ESC1

HI, I am currently doing a project with the B-G431B-ESC1. I am trying to control a motor with the B-G431B-ESC1. I already have profil my motor with the motor profiler software. I am able to control my motor with the motor pilot software. Now, I am tr...

elag by Associate
  • 2837 Views
  • 4 replies
  • 2 kudos