STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1740 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4887 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9585 Views
  • 5 replies
  • 3 kudos

Start a motor with sensor (using hall sensor) under heavy load situation, the motor will produce noise and motor sometimes can't move successful

I use MCSDK 5.3.2 and our board(which is similar IHM08h but we modify the over current from 30A to 60A) with using hall sensor to drive motor(our purpose is to drive E-bike and E-Scooter)But i find that in heavy load situation,i will hear motor will ...

SkyWork by Associate III
  • 1828 Views
  • 3 replies
  • 0 kudos

How to configure MCSDK for multiple motors?

Hello. I have done position control of single motor using P-NUCLEO-IHM03 with GM2804 + AS5048a(pwm encoder). And I hope to control 3 motors for gimbal. So I'm planning to design a board using the MCU and motor driver which are used in the P-NUCLEO-I...

wJang.1 by Associate II
  • 1585 Views
  • 2 replies
  • 0 kudos

Resolved! Relation between *.stmx file and drive_parameters.h ?

Often I find that MCSDK does not have the exact MCU I need to use so I need to end up modifying the CubeMx *.ico file generated from MCSDK.In trying to determine the relationship of these files I took an existing working project and renamed the *.stm...

BTrem.1 by Senior II
  • 1548 Views
  • 2 replies
  • 0 kudos

Resolved! MCSDK: ICS gain range is 5V but ADC only works with 3.3V

Hi! I am using F746ZG + IHM08M1. And I need configuration with 2 insulated current sensors.My question is why in Workbench ICS gain is in range from -5V to 5V where the ADC max working range ist only 3.3V. Which current sensors should I buy 3.3V or 5...

VKost.2 by Associate II
  • 2147 Views
  • 3 replies
  • 0 kudos

Resolved! EVSPIN32F0601S3 High Voltage BLDC Motor Drive:

Hi,1) How to run demo code for EVSPIN32F0601S3 (As parameters attached) ?2) When I have EVSPIN32F0601S3 eval board with me do I need only Enter Motor Parameters as in mcsdk to spin the Motor  (As parameters attached) ?Thanks in advance..--Karan