STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4882 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9582 Views
  • 5 replies
  • 3 kudos

Low-speed torque problem

Hi ST Community I used EVSPIN32G4 board and MC Workbench 6.2.1.I configured to use speed mode and hall sensor using EVSPIN32G4 sample project.The motor supports 15V, 16000rpm, and 40mN.And I tested it using MC_FOC_SDK GUI.The following situations occ...

Elliot95 by Associate II
  • 2483 Views
  • 4 replies
  • 0 kudos

Resolved! How to connect X-NUCLEO-IHM08M1 with NUCLEO-H563ZI?

Hello AllDoes anyone know how to connect X-NUCLEO-IHM08M1 with NUCLEO-H563ZI?I would to evaluate it with MC workbench 6.0.3.  However. I am not sure how to connect it together.It looks like I CAN'T plug it directly, because the slot and pins are not ...

yang2_0-1723707803038.png yang2_1-1723707839085.png
yang2 by Associate III
  • 1175 Views
  • 1 replies
  • 2 kudos

Resolved! Import a motor into Motor Control Workbench

Hi,I have emax cf2820 1200kv brushless dc motor and i want to drive it with X-NUCLEO-IHM07M1 motor driver and NUCLEO-G071RB control board. Since the motor I have is not registered in the workbench, I need to import it as a JSON file. Could you tell m...

Batuhan35 by Associate II
  • 4510 Views
  • 6 replies
  • 0 kudos

STM32 F0 + 6-Step PWM Glitchy - Need Advice

Hi there,I'm writing this post because I have encountered a potential bug/firmware issue with the MC firmware versions FW1.11.4/FW1.11.5 for the F0 fam, and I'm unsure on how to proceed in diagnosing the cause of this problem.Background:I want to use...

GustavEckerbom_1-1719836748322.png GustavEckerbom_5-1719840652627.png GustavEckerbom_6-1719841745950.png