STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1725 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4873 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9558 Views
  • 5 replies
  • 3 kudos

Resolved! MC Workbench Phase Voltage Sensing

Hello,I am designing FOC motor controller based on DRV8316. For this, I am adding a DRV8316 custom board in the MC Workbench. Please find the JSON file attached. The problem is that I am unable to add phase voltage sensing. Although I have added phas...

farzansaleem_0-1724785407643.png farzansaleem_1-1724785424396.png farzansaleem_2-1724785589618.png

how to implement ENCODER MoDE using GPIO ?

In my design , MCU controll 8 sets of  STEP MOTOR  .    Every MOTOR  has  A / B Encode pulse outputsIN CubeMx  Six timers (TIM1-TIM5  & TIM8  )can be configured to ENCODER MODE 。  But  How to implement the other 2 Motors decoder ?   Can we use gpios ...

JohnGe by Associate
  • 1002 Views
  • 1 replies
  • 0 kudos

PA9/10 Remapping feature on MC Workbench?

Hi, I've been using my custom board with the STM32C011G6 MCU as a control board. By customizing the JSON file on the power board, I've been able to generate a project through MC Workbench -> CubeMX -> CubeIDE, and the motor driver has been running we...

Resolved! Low-speed Motor Control Solution - ZeST algorithm

Hello ST,I’m a motor control fan and developed a few motor controllers in the past years for myself. I always worked with TI MCU’s because I liked their sensorless solution for PMSM control. At low speed the torque generation was not bad but at zero ...

MDani by Associate II
  • 4410 Views
  • 5 replies
  • 0 kudos