STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1743 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4892 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9594 Views
  • 5 replies
  • 3 kudos

HSO Evaluation Problems

Dear All,My platform as list:Control Board: B-G473E-ZEST1SPower Board:  STEVAL-LVLP01  Motor: B-MOTOR-PMSMA1Platform: MCSDC 6.3.0,  (I attached my Workbench configuration file as follow)CubeIDE: 1.15.1  When I try to evaluate the HSO, the Motor pilot...

yang2_1-1725866298825.png yang2_0-1725866291229.png
yang2 by Associate III
  • 1223 Views
  • 1 replies
  • 0 kudos

ST Motor Control Source Code generation fails

Hello,I have buy the NUCLEO-F302R8 board with the X-NUCLEO-IHM07M1 with the motor BR2807. Now I search for the library and code generation with STM32CubeMX. It is stand on the web page that is "Workflow supporting the STM32CubeMX GUI configurator". B...

bm2_0-1725542595196.png
bm2 by Associate III
  • 1300 Views
  • 2 replies
  • 0 kudos

Resolved! EVSPIN32G4 - Frequent Overcurrents

Hi.I'm driving a PMSM with FOC (Workbench file attached for reference) with MCSDK 6.3.0 in torque mode.Main parameters:1400 Hz electrical frequency max -- therefore 16 kHz PWM100 Hz mechanical frequency max~0.03 mH line-to-line inductance~9 V/Hz Kv 0...

grisharevzin_0-1723900399238.png

ST motor pilot V1.2.9 localisation issue

The GUI MC_FOC_SDK is supposed to be able to tune revup parameters. However, if we try to modify variables in the Torque-column (and only in this column), all input is reset to zero:I have tracked the issue down to RevUpComponent.qml -> doublespinbox...

LLang_1-1725367773199.png
LLang by Associate
  • 1191 Views
  • 1 replies
  • 3 kudos

Resolved! Lecture registre HALL_EL_ANGLE ou HALL_SPEED

Bonjour,    J'ai configurer le contrôle moteur avec un capteur effet hall en auxiliaire.le moteur tourne mais les valeur des registre ne change pas. elle prennent une valeur différente a chaque démarrage mais ensuite ne change jamais. Comment vérifie...

Christophe65_1-1724751831609.png