STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1725 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4873 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9561 Views
  • 5 replies
  • 3 kudos

Engine stops after a few seconds.

Hello everyone.I am using the Motor Control WorkBench 6.3.0 application to generate the project. The inverter board isB-G431B-ESC1. The motor is a 2-pole BLDC, 8.5V, it has a very low inductance of 0.04mH, an Rs of 0.37ohms and the B-Emf constant is ...

OttoBCN by Associate II
  • 3601 Views
  • 8 replies
  • 0 kudos

Reset issue STSPIN32F0A

Hello,I have some troubles with the STSPIN32F0A when the load on the motor increases,the STSPIN will reset. The reset cause is checked in firmware at startup, and the cause mentioned is RCC_FLAG_PINRST.Apart from a pull-up and a capacitor to ground, ...

CCarl by Associate II
  • 2316 Views
  • 5 replies
  • 0 kudos

ADC2 configuration issue (injection and regular)

Hi,The version of mcsdk I'm using is 6.3.0, I have a problem with my ADC2, enabling one injection channel as a sample of phase current, and three regular channels, one of which is used as a speedpotentiometer, and two for my own use, and currently ru...

iskan by Associate III
  • 835 Views
  • 0 replies
  • 0 kudos

Resolved! evspin32f0602s1 Motor driving C code

Hello, I am very new for ST mc. I want to use evspin32f0602s1 for BLDC motor,I have generated the code using Workbench,STCubemx and finally code seen in IDE,but I dident getting what to write in main() function ,how it can handle any fault situation ...

KVijay32 by Associate II
  • 1437 Views
  • 2 replies
  • 0 kudos

Hardware Flow Control in CubeMx selection

How to enable Hardware Flow Control in STM32 Cube MX , because when I am trying to enable it - conflict with ADC1:IN6 . I want to enable Hardware flow control RS485. I have attached the screenshot of the issue being faced. This program is generated ...

Screenshot (96).png
hu88 by Associate II
  • 1285 Views
  • 1 replies
  • 0 kudos

Resolved! MC 6.3 with MX6.12 - attr not supported : Dmpu

I am trying to generate code for "STM32 Nucleo packs FOC and 6-step motor control platform for three-phase, low-voltage and low-current motor" and I keep getting errors :-Attr not supported : Dmpu  as in attached image. I am using cubeMX12, I have up...

mc.JPG
Sujoy_B by Associate II
  • 17088 Views
  • 18 replies
  • 4 kudos