Skip to main content
Visitor II
March 14, 2024
Question

X-Nucleo-IHM03A1

  • March 14, 2024
  • 1 reply
  • 609 views

Good morning

I am in the process of building another CNC milling machine. For the two largest stepper motors , I would like to use X-Nucleo-IHM03A1 drivers connected to the Stm32 board. I initially looked at the capabilities of IHM03A1 and batch files for Stm32CubeIDE.

I have a question:

Can IHM03A1 be controlled via Stm32 board from an external motion controller , for example by providing an external PULSE signal to the STCK pin ?

Thank you in advance

    1 reply

    Peter BENSCH
    ST Technical Moderator
    March 15, 2024

    Welcome @Janusz53, to the community!

    Which STM32 board did you connect the X-NUCLEO-IHM03A1  to? If it is a NUCLEO board, you should be able to use it to control the X-NUCLEO?

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.