2024-02-24 3:08 PM
I am running a 28 pole 20A nominal motor using x-Nucleo IHM08M1 and a nucleo -G431RB. I have been doing a number of tests verifying locked rotor current/torque and checking the effect of different settings of proportional gain.
I am using Stm32CubeMonitor to monitor all the variables.
I am using 6 step control. and Hall devices for sensing
My understanding seems to be progressing. answers to the following two questions would assist me greatly.
1/ When I use the following code to monitor the speed
MC_ProgramSpeedRampMotor1(1,0);
MC_StartMotor1();
for (int i = 1; i <= 200; i++)
{
Faults =MC_GetOccurredFaultsMotor1();
speed = MC_GetAverageMecSpeedMotor1_F();
HAL_Delay(50);
}
MC_StopMotor1();
I get integer values for speed and in multiples of 6. eg the speed value jumps from 0 to 6 to 12 etc whereas I am expecting a float as an answer.
The final speed is 36 rpm whereas I expect it to be 6 rpm.
What am I doing wrong?
2/ At 28 poles x 6 steps gives me 168 positions per rotation and with a 300 mm Outside diameter rotor I expect to be able to do position control giving me approximately a 3mm resolution.
How do I single step this motor or move it a set number of steps.
Thanks
Roy
Solved! Go to Solution.
2024-03-14 12:30 AM
Clearly I am not getting any response to this question. So I will close it off. With regard to the speed being integer values in multiples of 6 I think this is related to the speed unit of 0.1Hz which is 6rpm. So I will ask the question again in a new post and hopefully will get a response.
2024-02-29 10:22 PM
Could some kind soul point me in the right direction on this - thanks
2024-03-07 12:47 AM
Can AnyBody help?
2024-03-14 12:30 AM
Clearly I am not getting any response to this question. So I will close it off. With regard to the speed being integer values in multiples of 6 I think this is related to the speed unit of 0.1Hz which is 6rpm. So I will ask the question again in a new post and hopefully will get a response.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.