STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1732 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4880 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9575 Views
  • 5 replies
  • 3 kudos

Resolved! Clock configuration question

Dear Sir,When I configure the clock for the STM32H5, I found that the CPU Clock doesn't match the actual result of the dividers. For example, in the figure showing my current configuration, considering the red path, my clock source is from HSI (64/2 ...

yang2_0-1726111035715.png
yang2 by Associate III
  • 1244 Views
  • 1 replies
  • 0 kudos

Motor Control Profiler support for EVALSTDRIVE601

Hi,I am having STM32 Nucleo-64 development board and wanted to have it used for high voltage BLDC motor drive. For that, I have below boards:https://www.st.com/en/evaluation-tools/nucleo-g474re.html https://www.st.com/en/ecosystems/x-nucleo-ihm09m2.h...

mdalal by Associate III
  • 896 Views
  • 1 replies
  • 0 kudos

Motor Control MCU change

 Hello everyone,I am trying to transfer my project generated with motor control workbench from a STM32G431 to STM32G473. Thus, using CubeMX, I opened a new project with the STM32G473VET device and then imported the project generated with the workbenc...

carlos_gtronix_0-1725987482147.png

Resolved! Motor profiler bugs

Hello,I'm playing with a nucleo-F446 + IHM16M1.The MC workbench is able to generate code. I am able to compile and program it using cube IDE. Running the default Gimbal motor with the standard parameters is still painfull. I'm trying to get a better ...

tarzan by Associate II
  • 2863 Views
  • 3 replies
  • 1 kudos