cancel
Showing results for 
Search instead for 
Did you mean: 

Schematic for stspin32 and mosfet recommendation

kavinkumar
Associate III

Hi Guys

I'm just a newbie who got into stm32 architecture and i want to develop a BLDC controller for a Flycat 5010 360kv BLDC motor the power supply is 24v and the max current rating i want is 60A can anyone recommend me a schematic a application note to hook up the MCU and Recommend a mosfet to handle the above mentioned spec any help would be appreciated.

Thank you

Kavin kumar

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Gael A
ST Employee

Hello kavinkumar,

Currently the MCSDK supports very few boards that can sustain such current levels, and seeing the kind of motor you want to use, I can't help to wonder if that is really necessary. Would you be so kind as to elaborate on the type of application you want to go into ? Is the board only meant for motor control ? Are you planning on running several of these motors on the same board ?

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.
kavinkumar
Associate III

I want to make FOC Bldc controller board for a Quadruped robot where each motor has a separate Mcu and only one motor will be driven under one MCU