STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 Ethernet Not Working

Hi There,I am trying to run the ethernet example from the 1.7.0 version of the STM32H7 firmware at STM32Cube_FW_H7_V1.7.0\Projects\NUCLEO-H743ZI\Applications\LwIP\LwIP_HTTP_Server_Netconn_RTOS.The only modifications I have performed from the provided...

PMart.1 by Associate III
  • 12729 Views
  • 29 replies
  • 1 kudos

I ported an application from STM32L496RG to L4Q5. Most of application is working except the ADC acquisition because of DMA and the new DMAMUX1. I used the LL ST library unfortunately I didn't find any LL example of ADC + DMAMUX. Could you give examples?

ADC in dual mode with sampling frequency of 10.66 MS/s (5.33 per ADC).The System clock is set to 120 MHzThe ADC clock is set to 80MHzThe ADC1 IN8 ext3 is trigged by TIM2 CC2.The ADC data transfet is done though DMA2 CH3

Resolved! STM32G431 UCPD continuous power cycling

Hi,I'm developing an USB-C sink, using dead battery feature.I have respective CCx pins connected to DBCCx pins and the source can successfully power the sink.However, when the UCPD code starts running, the source disconects the 5V, effectively result...

STM32F769i-DISCO Ethernet Speed

Hello,I am using STM32F769i-DISCO board in my project. The project include camera module and I get data from this module using DCMI. I want to send this data to computer via ethernet. For this I need at least 100Mbits/s ethernet speed. But I cant f...

Baris by Associate
  • 701 Views
  • 0 replies
  • 0 kudos

STM32H747 USB CDC device not detected

I have an STM32H747I-DISCO board and try to connect it to a computer as a USB CDC device.I use CubeMX to configure the USB (USB_OTG_FS in Device_Only mode, USB_DEVICE_M7 with CDC class, 48MHz clock for the USB peripheral) but when the generated progr...

gv by Associate
  • 1688 Views
  • 1 replies
  • 0 kudos

I have the STM32446e board. I've been trying to get any sort of analog mic input working through the onboard WM8994 codec. None of the provided examples support this. Hardware background, so I'm confused by all the drivers. Any easy way to do this?

The examples only support the digital MEMS microphones on the board. I'm uncertain whether the BSP actually supports using analog in. The wm8994.c driver supports analog in, but I'm not certain this function is actually being called by the higher abs...

CMcBa.1 by Associate
  • 882 Views
  • 0 replies
  • 0 kudos