STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 USB custom class

Hi,I want to use my own custom usb device class base on usb core provided by ST. Inspecting the code, I found that "DataIn" and "DataOut" callback functions provided by the class to usb core are called at the END of the data in or out stage... Callin...

Getting sleep to work when USB CDC is enabled?

My program has the option of sleeping for a period using the RTC to wake or sleeping until the wakeup pin is set high. Both these functions work perfectly if I talk to the outside world using a uart.However, I configure CDC as a serial port SLEEP doe...

PMath.4 by Senior III
  • 5474 Views
  • 13 replies
  • 0 kudos

STM32L4R5 Flash programming and dual bank switch

Hello community,I'm currently having issues or perhaps not fully understanding the procedure of writing data to the MCU bank 2 and then switching to this bank to run the program from bank 2.My setup for now is using a custom protocol for sending the ...

Ajoha.2 by Associate
  • 1002 Views
  • 1 replies
  • 0 kudos

Confused about F407 USB OTG FS

I wanted to implement a simple USB device only on a STM32F407. When I enable it in CubeMX under USB_OTG_FS I get a DP and DM line and there is an option to activate the VBUS line. Is activate VBUS absolutely necessary? It is after a simple device onl...

Resolved! Ethernet example modification for STM32H745I-DISCO

I came across this Ethernet example:https://community.st.com/s/article/How-to-create-project-for-STM32H7-with-Ethernet-and-LwIP-stack-workingIt is giving me an issue regarding configuring HSE in bypass mode. The maximum core frequency l can get is 96...

DWill.4 by Associate II
  • 1725 Views
  • 4 replies
  • 0 kudos