STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! A Mistake Found in HAL Library

Function "PWM Generation CH2N" can not work, channel CH2N don't output PWM signal. But after I changed "tmpccer &= ~TIM_CCER_CC2NE;" to "tmpccer |= TIM_CCER_CC2NE;" (in file stm32h7xx_hal_tim.c), it works well.Hoping developers of HAL library will fi...

Laurie1 by Associate III
  • 2447 Views
  • 4 replies
  • 0 kudos

LwIP Build Analyzer

Hey there,I have a question regarding the output of the build analyzer. When I set up freeRTOS + lwIP , like explained here: https://community.st.com/s/article/How-to-create-project-for-STM32H7-with-Ethernet-and-LwIP-stack-working on my STM32H753 eve...

0693W00000D0hLKQAZ.png 0693W00000D0hMqQAJ.png
ESawa.1 by Senior
  • 1961 Views
  • 5 replies
  • 0 kudos

Facing CRC checksum issue with STM32CubeIDE, it doesn't generate automatic checksum what are the steps need to follow generate checksum and attach end of the application. Do i need do any configuration in linker file Flash.ld ? please help me.

i am integrating STL XCUBE class-B 2.2.0 Packages with STM32L433 controller here issue with CRC test failing, what are configuration required to generate checksum attach end of application.This patch i found in the SWSTM32 IDE linker file  /* check ...

NPULI.1 by Associate II
  • 3516 Views
  • 3 replies
  • 0 kudos

SDMMC_GetCmdResp1(); bug

Hi,My programme of Write/Read from an eMMC is buged in this function call :static uint32_t SDMMC_GetCmdResp1(SDMMC_TypeDef *SDMMCx, uint8_t SD_CMD, uint32_t Timeout){ uint32_t response_r1; uint32_t sta_reg; /* 8 is the number of required instructions...

PyKe by Associate III
  • 1412 Views
  • 1 replies
  • 0 kudos

Resolved! which USART can I use for bootloader?

I can see in the datasheet of STM32G474CE that I can use USART for reprogramming the Flash memory, but I am trying to understand which one?In STM32F4 I can use USART1 and USART2, is it the same here?Thanks.

NZube.1 by Associate
  • 1422 Views
  • 3 replies
  • 0 kudos