cancel
Showing results for 
Search instead for 
Did you mean: 

I want to wakeup from standby-mode in less than 20msec.

YTaka.1
Associate

I want to wakeup from standby-mode in less than 20msec.

I want to wake up from standby-mode in less than 20 seconds using Periodic auto-wakeup, but I can't wake up below 22 msec.

Could you tell me if there is any good way?

The following HAL driver is used.

HAL_RTCEx_SetWakeUpTimer( & hrtc,1,RTC_WAKEUPCLOCK_RTCCLK_DIV2 );

And the MCU is STM32L433.

Thanks in advance!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
M.Hajji
Associate III

Hello YTaka.1

First make sure your LSE/RTC is well calibrated, you can use the 1Hz RTC_output to be sure of that.

In RM0394 section 36.3.6 Periodic auto-wakeup, it say "When the periodic wakeup interrupt is enabled by setting the WUTIE bit in the RTC_CR register, it can exit the device from low-power modes." So I guess give HAL_RTCEx_SetWakeUpTimer_IT a try.

I suggest also to test, without entering the standby mode, the time between two wakeup event by the RTC, just to better understand how your system behave.

Good luck,

Regards,

Hajji.