2020-08-29 8:18 AM
Hello, I have an project with STM32F103 and using CubeMX drivers. I successfully setup the driver, but I have a problem when trying to send out from pc packets biggest than 64 bytes. (64bytes is the enpoint buffer & max packet size). On PC I'm using simple testing program which sends packets with different lengths from 10bytes to 200bytes. Expected behavior is that interrupt occurs for every 64bytes, then the buffer is swapped and next packet is received, but this is not working as expected.
My registers settings:
CNTR: 0xBF00
EP0 - CONTROL RX/TX
ADDR_TX: 0x58
COUNT_TX: 0x0
ADDR_RX: 0x18
COUNT_RX: 0x8400 (only setting)
EP1 - DATA IN (Single buffered)
ADDR_TX: 0x98
COUNT_TX: 0xAD
ADDR_RX: 0xA0BA - not cleared, but not used...
COUNT_RX: 0x800 (only setting)
EP2 - DATA OUT (Double buffered)
ADDR_TX: 0x118
COUNT_TX: 0x0
ADDR_RX: 0xD8
COUNT_RX: 0x8400 (only setting)For transfers from 10 to 60 bytes everything works nicely:
INT: USB_EP2R: 0xF142 count: 10 countPma0: 10 countPma1: 0 USB_EP2R: 0x7102
INT: USB_EP2R: 0xB102 count: 20 countPma0: 0 countPma1: 20 USB_EP2R: 0x3142
INT: USB_EP2R: 0xF142 count: 30 countPma0: 30 countPma1: 0 USB_EP2R: 0x7102
INT: USB_EP2R: 0xB102 count: 40 countPma0: 0 countPma1: 40 USB_EP2R: 0x3142
INT: USB_EP2R: 0xF142 count: 50 countPma0: 50 countPma1: 0 USB_EP2R: 0x7102
INT: USB_EP2R: 0xB102 count: 60 countPma0: 0 countPma1: 60 USB_EP2R: 0x3142But for 70bytes transfer I got:
INT: USB_EP2R: 0xF142 count: 64 countPma0: 64 countPma1: 0 USB_EP2R: 0xB102
INT: USB_EP2R: 0xB102 count: 0 countPma0: 0 countPma1: 0 USB_EP2R: 0x3142So it seems that the interrupt is called nicely, but the count registers are empty for the second part of the transfer. I can't figured out what is going wrong. Can anybody help me with this strange problem?