STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H745 ethernet - problem pinging

Hello,We are designing a system based on a STM32H745ZI. Functionality includes TCP communication.Just for start, I've implemented LWIP based design on the Nucleo144-745ZI board.It's based on example from https://community.st.com/s/article/How-to-crea...

stm32h7 using eth mac

now,I using stm32h7 series, and run eth mac to trasmit and receive ethernet frame. but It can trasimit ethernet frame sucess,but It can`t receive.I had set mac filter to receive all.the program:static void MX_ETHMAC_Init(void){ ETH_MACFilterConfigTyp...

gcaif by Associate II
  • 1828 Views
  • 2 replies
  • 0 kudos

Resolved! Promiscuous Mode

Hi I want to use Promiscuous Mode with LWIP+STM32H743.I want to be able to capture frames not sent over to my IP address.Is it possible?Thanks

deckhard by Associate III
  • 3689 Views
  • 8 replies
  • 0 kudos

Resolved! STM32H753 Ethernet stop working

we have several device with STM32H753, and they are talking to each other, over LwIP.one of the devices is the master who charges on the protocol communication between all other peripheral devices.the master send a ack message to each device in a loo...

Lmali.1 by Associate III
  • 2616 Views
  • 5 replies
  • 0 kudos