STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_CAN_AddTx Message returns HAL_CAN_ERROR_PARAM

Hi everyone,I am working with STM32F405 and trying to transmit 16bit data using CANBus line including several units (motor controller, Bms and other circuits). Our CANBus line works fine for a long time. Now I am trying to add one more device to our ...

Myurt.1 by Associate
  • 1682 Views
  • 1 replies
  • 1 kudos

USB CDC (Device) working with FreeRTOS on the STM32769I-DISCO. Does ST have example code of these two working together ?

I note that the XCube-AWS software employs FreeRTOS as a task scheduler. I'm using the STM32F769NI-DISCO development board to do some testing. That software is working out of the box. I can see the Ethernet handled as a task. I also see the USB CDC (...

Battery-powered STM32L4 Discovery kit (B-L475E-IOT01A) ST_LINK chip will not allow code to execute unless plugged into USB port.

Hello,I've built a project with the B-L475E-IOT01A Discovery Kit that is intended to be a battery-powered stand-alone unit. I've wired it to be powered via the 5V Arduino header and set the 5V jumper appropriately. However, the unit will not start ex...

PSche.4 by Associate
  • 3237 Views
  • 4 replies
  • 0 kudos

osDelay failed

I am working with stm32h753zi board and i am tring to implement the task swithcing logic, if task 1 is running task 2 wait on while loop and while task 2 is running task1 should wait of while loop. I task 2 locked inside the osDelay().

AFaya.1 by Associate III
  • 1894 Views
  • 2 replies
  • 0 kudos

Resolved! Application doesn't work when loaded through USB DFU

Hello,I am working on the USB DFU for a STM32H7A3ZGT6I have two projects one for the DFU and one with the application to be updated.My application works fine when I download it with the debugger.The DFU part manages to erase and program the new app t...

ABricout by Associate III
  • 2767 Views
  • 6 replies
  • 0 kudos