cancel
Showing results for 
Search instead for 
Did you mean: 

How can I install the X Cube Audio Package 1.1.1 into STM Cube MX ?

mo'br
Associate

When I click on install or remove embedded software packages, using both install from local and use URL fail. When I have the package zip file local I get the error "The given file is not recognized as beeing (spelt wrong!) valid. It must either be a MCU or CMIS pack". So I presume I do something else with this expansion pack as its not a MCU or a CMIS ? 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Houssem CHAABANI
Senior II

Dear @mo'br​ ,

Could you please share the .ioc file and try to use the last available version of STM32CubeMX.

Kind regards,

Houssem

cmdr
Associate

I have the same problem. I tried CubeMX version 6.1.1. I don't have an .ioc file because this happens before creating a project.

I'm also wondering why the Audio package does not appear in the list in the Embedded Software Packages Manager along with the other X-CUBE-* entries.

x893-00
Associate II
  • It `s Magic

ST programming guru's answer