Browse
STMicroelectronics Community
FAQs
Sign In
Product forums
STM32 MCUs
STM32 MCUs products
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
STM32 MCUs Other solutions
STM32 MPUs
STM32 MPUs products
STM32 MPUs Boards and hardware tools
STM32 MPUs Software development tools
STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
Microcontrollers
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
Ganesh.T
Associate II
since
2020-12-28
2023-08-01
User statistics
8
Posts
0
Solutions
0
Kudos given
0
Kudos received
View all badges
STMicroelectronics Community
About Ganesh.T
Options
Report User
User Activity
Posts
Replies
How to keep u-boot splash display during kernel booting ?
2021-10-27
I can able to display splash image from uboot. but once kernel boots it will disappeared, screen will become black . So i want avoid framebuffer clear of dispaly.
Is it possible to send 2048 bytes in tcp in lwip at single write? MCU : stm32F407
2021-08-02
SPI Read in uboot - SPI2
2021-05-06
Hi ,Actally i want to read a PISO shifht register as spi slave.Device Tree: spi2_pins_a: spi2-0 { pins1 { pinmux = <STM32_PINMUX('A', 9, GPIO)>, /* uart8_tx */ <STM32_PINMUX('I', 2, GPIO)>, /* uart8_tx */ <STM32_PINMUX(...
How can i reduce stm32MP1 bootup time further? im expecting to it shoulf boot within 16 sec ?
2021-04-28
systemd-analyze blame: 6.297s dev-mmcblk1p3.device 3.711s user@0.service 3.668s systemd-udev-trigger.service 729ms console-kit-log-system-start.service 663ms weston.service 598ms systemd-logind.service 516ms pxl-in...
Is STM32MP157CAAx support MS-DOS partition type ? or it will support only GPT type ?
2020-12-28
Re: STM32MP157f-dk2 'drm-backend' has not been destroyed.
2023-07-31
Hi,Im getting same error in weston-launch. Can someone help ?
Re: How to keep u-boot splash display during kernel booting ?
2022-02-24
Hi @Community member :Yes.., Something similar.,But here i want to keep Uboot splash till my application comes up.
Re: STM32MP157AAC Secure Boot Process on Avenger96 board
2021-02-16
Hi,Im also facing same issue in spi2 - uboot to PISOSR shift register ..Please help on this...