STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FreeRTOS libraries for USB audio dongle.

Hello, For the B-U585I-IOT02A device with FreeRTOS, I want to plug an USB audio dongle into the board, and want to get/put audio data from/to the USB audio device, but when I searched the FreeRTOS APIs, it seems that there's no standard APIs for gett...

IChoi.2 by Associate
  • 1400 Views
  • 1 replies
  • 0 kudos

I2C Master send incorrect data

STM32F103C8Cube IDE 1.10Greeting,I tried to send data (count from 13 to 15 every 500ms) thru i2c1 using HAL_I2C_Master_Transmit.slave is pcf8574, scl & sda line pulled up with 3k3 resistor.usb scope shows master send correct address, but data always ...

Arobb.1 by Associate
  • 2731 Views
  • 4 replies
  • 0 kudos

Hard fault on I2C library interrupt

Hello everyone,I encountered a weird situation concerning I2C on a project at work. We are using an STM32H743XIH6.We have an I2C device sending data, the I2C is setup with a DMA. Everything works fine until we have a physical disconnection of the I2C...

0693W00000QNNFdQAP.png 0693W00000QNNFxQAP.png 0693W00000QNNFZQA5.png
MSchö.1 by Associate
  • 989 Views
  • 0 replies
  • 0 kudos

[BUG_REPORT] Incorrect handling of SPI interrupts.

Current implementation of the SPI transmit HAL function handles incorrectly interrupts. Actually the interrupt handler is implemented like this:static void SPI_TxISR_8BIT(struct __SPI_HandleTypeDef *hspi) { *(__IO uint8_t *)&hspi->Instance->DR = (*...

AGime.1 by Associate II
  • 1452 Views
  • 2 replies
  • 0 kudos