cancel
Showing results for 
Search instead for 
Did you mean: 

Is HAL_SPI_Transmit_DMA faster than HAL_SPI_Transmit?

DMårt
Lead

Hi!

Is HAL_SPI_Transmit_DMA faster than HAL_SPI_Transmit?

If yes: Do I need to enable DMA for the SPI to make this work?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
PMath.4
Senior III

Setting up DMA takes time so will always be slower for small transfers. For larger transfers DMA is better but only if there is something else you want to do while the transfer is happening. Otherwise speed will be the same.

View solution in original post

7 REPLIES 7
Rookie38
Associate III

Hello,

Yes, transferring larger amounts of data is faster using DMA. The data transfer process is outsourced to the DMA controller and the MCU can continue working. Again, yes, DMA must be configured for use with the specific SPI bus. You should give a look at the CubeRepository examples:

For example for STM32F4 Series:

..\STM32Cube\Repository\STM32Cube_FW_F4_V1.26.1\Projects\STM32F429I-Discovery\Examples\SPI

There are three examples for SPI communication via polling, interrupt and DMA available.

Thank you. I tried with HAL_SPI_Transmit_DMA and it was much slower than HAL_SPI_Transmit.

In this case, I transfered maximum 1 to 4 bytes of data.

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer

Your question isnt right. Speed of SPI is defined aka clock. Little change is interword times when is used IRQ vs DMA.

Your code must have fail when dont work...

Yes. But isin't DMA SPI the same as regular SPI without time out?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer

Speed is same because SPI have FIFO

PMath.4
Senior III

Setting up DMA takes time so will always be slower for small transfers. For larger transfers DMA is better but only if there is something else you want to do while the transfer is happening. Otherwise speed will be the same.

So there no reason to call SPI_DMA then if I want to transmit data?

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

STM32MP257FAK3 custom board with STM64-OS as operating system: https://github.com/DanielMartensson/STM64-Computer