STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Custom HID transfer big size data failed

I'm trying to use High speed USB HID to transfer bulk data from external SDRAM controlled via FMC.I have achieved the basic transfer function by modifying the USB description file and related functions.​ /******************** Descriptor of Custom HID...

LioChen by Associate II
  • 4305 Views
  • 7 replies
  • 0 kudos

Resolved! STM32F7: new (2022-07) ethernet HAL - anybody tested it?

Heyho,has someone already tested the new HAL ethernet driver for F7 ?I have my F767 prototype up and running, raw lwIP with http server and PTP are working flawlessly.After having done lots of other driver and user interface via http / REST stuff, I ...

LCE by Principal II
  • 4086 Views
  • 6 replies
  • 0 kudos

How to get STM32H743I-EVAL2 working with GUIX?

 I was looking for h/w to start development of a AzureRTOS GUIX app that also had the I/O including multiple A2D, GPIO, and serial communications. Based on a various ST Micro presentation and a review of the specs, I though the STM32H743I-EVAL2 migh...

FKoops by Associate
  • 1321 Views
  • 2 replies
  • 0 kudos

Combining CAN2 and USART2

Hello,At the moment I'm working on a project using the STM32F4 discovery board that combines CAN2 and USART2. I managed to get them both working separately, but when I combine them in the same problem I get weird output on the serial monitor. When I ...

Rde K.1 by Associate III
  • 1628 Views
  • 2 replies
  • 1 kudos