STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C read specific register without repeated start

Hello,I'm interfacing the KTD2026 RGB sensor.Writing to the device's registers works with normal HAL I2C functions.The problem i'm facing is reading the device's registers which from datasheet should be done the following way:I have tried both HAL_I2...

0693W00000Y85fQQAR.png
CBras by Associate II
  • 1676 Views
  • 3 replies
  • 0 kudos

HAL_FLASH_OB_Launch() Hangs STM32L5

I'm attempting to enable the SRAM2 parity bits on an STM32L552, and any time I call HAL_FLASH_OB_Launch, the chip hangs. I've also tried directly setting the OBL_LAUNCH bit in the NCSR register with the same results.I've looked through some of the L...

MBand.3 by Associate III
  • 3418 Views
  • 3 replies
  • 0 kudos

How to use UART DMA RX?

Hello.​I developed UART by DMA method and it works normally, but I am posting because I have one question.​In the case of the sites I found, most of the main function or initial HAL_UART_Receive_DMA function was called, and the HAL_UART_RxCpltCallbac...

0693W00000Y83ErQAJ.png
JLEE.211 by Associate
  • 2840 Views
  • 2 replies
  • 0 kudos