STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer activation in ThreadX causes Hardfault

Hi all,I'm trying to get a TouchGFX application running. I'm controlling a 16bit TFT LCD through FMC (16 lanes) with my Nucleo U575ZI-Q. As I'm using a custom LCD driver, I set both the Interface and the Application Tick Source to 'custom' in the .io...

MGuth.1 by Associate III
  • 2247 Views
  • 1 replies
  • 0 kudos

operating & storage environment

STM32F429ZIT6USBLC6-4SC6STM32F091RBT6Please tell me about this content.1)operating environment (temperature, humidity, vibration resistance, location)2)storage environment (temperature, humidity, vibration resistance, location) 

thoso.1 by Associate
  • 1176 Views
  • 1 replies
  • 1 kudos

Custom bootloader for dual-core STM32H745ZI

I made custom bootloaders for STM32F7 and SM32H7, so I'm a bit familiar with the process to update an application when using a bootloader.But how does one make a bootloader for a Dual-Core STM32H7?I think it goes like this.If I use the CM4 core for t...

Jack3 by Senior III
  • 1880 Views
  • 3 replies
  • 2 kudos

What if i debug the STM32f429iit6 program in Nucleo F429zit6 ?? I debug it in nucleo and now nucleo's USB FS working fine but the same code does not working in controller(stm32f429iit6). why this is happening ??

I have two boards Nucleo F429ZIT6 and STM32F429IIT6 . Both controller have same Data sheet , both have same USB FS pin. I write the code for stm32F429IIT6 and debug it in both of boards my nucleo board is working fine but my STM32F429iit6 board is no...

pshin.2 by Associate II
  • 3383 Views
  • 8 replies
  • 0 kudos