STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi everyone, I'm looking to design and develop a USB Audio Interface using STM32F4xx series MCUs that could ideally record up to 16 channels of analog audio signals, convert and send to a PC / MAC via USB.

If anyone is familiar with Digital Audio Workstations (DAW's), you can then select the type of audio input device in the application, to then choose which channel to monitor and record.I'm familiar with the process of how to record the incoming audio...

cackland by Associate
  • 2823 Views
  • 3 replies
  • 2 kudos

STM32H747I with LWIP not working

HelloI used the STM32H747-Disco development board and created a Keil project according to this link, https://community.st.com/s/article/How-to-create-project-for-STM32H7-with-Ethernet-and-LwIP -stack-workingMy CubeMX is version 6.6, and the firmware...

YZhen.4 by Associate II
  • 2854 Views
  • 4 replies
  • 0 kudos

ST ROM Bootloader boot0 pin

How is the boot0 pin is intended to be used by ST chip designers in real world applications? Once the boot0 pin is set high, the chip executes the bootloader section in memory and it will not go back to the execution of application section of memory ...

KoS by Associate
  • 4526 Views
  • 4 replies
  • 0 kudos

STM32F722: USB Device peripheral: HID: When connected through a USB hub to a Windows 10 host PC, how are OUT transactions addressed to a different device handled

STM32F722: USB Device peripheral: HID: When connected through a USB hub to a Windows 10 host PC, I can see endpoint data (OUT transactions) with another device address present before the Set_Address is issued by the host. There are other active devic...

MLyon.1 by Associate
  • 1051 Views
  • 0 replies
  • 0 kudos

Timer activation in ThreadX causes Hardfault

Hi all,I'm trying to get a TouchGFX application running. I'm controlling a 16bit TFT LCD through FMC (16 lanes) with my Nucleo U575ZI-Q. As I'm using a custom LCD driver, I set both the Interface and the Application Tick Source to 'custom' in the .io...

MGuth.1 by Associate III
  • 2245 Views
  • 1 replies
  • 0 kudos