STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The USB VBUS doesn't work. It is not recognized.

I've been programming with a STM32F407G, but the USB VBUS doesn't work. It is not recognized by my computer. It connects and disconnects. I changed the micro USB cable, I updated the firmware of the board, I tried to connect the board in another comp...

_legacyfs_online_stmicro_images_0693W00000bkhJpQAI.png
MAlon.2 by Associate
  • 2459 Views
  • 3 replies
  • 0 kudos

Performance of the AzureRTOS TCP sockets is mixed - I see high socket connection losses when running this TCP socket connect loop code. Do you have any suggestions to improve the socket handling of this code?

Attached is the test code for the tcp socket loop test. I have seen very high failures up to 26 failures out of 40 tcp socket create/connect attempts.

JVand.12 by Associate II
  • 1335 Views
  • 0 replies
  • 0 kudos

Bad board or bad debugger?

Hi,I have a B-L475e-IOT01A1 board. I have been trying to learn FreeRTOS with this board. I am using STM32CubeIDE v1.12.1. When I simply load an application onto the board, it appears to load properly. However, when I try to run my code through th...

jmazz.1 by Associate II
  • 2801 Views
  • 6 replies
  • 0 kudos

STM32G431C8T6 SPI bootloader whole-chip CRC cmd was acknowledged but address after that received neither ACK or NACK

my host interaction with STM32G431C8T6 SPI bootloader are functioning for a lot of jobs such as RW, but not for the whole-chip CRC. Here is the Logic analyzer captured data:Host=>BL, BL=>Host5A, A5A1,A55E,A5 cmd to run whole chip CRC00,A5......00,A50...

pxia.1 by Associate II
  • 996 Views
  • 0 replies
  • 0 kudos

STM32U585 unexpected USB_RST

Hi,i have a STM32U585 MB1551C board running with a custom software.I have a tinyusb stack up and running. The device successfully appears as a vcom port on a windows pc.But unfortunately after some time, round about 10-20sec., I get another USB_RST i...

How to apply for a USB PID

Hi.We are developing a product that will use USB on an STM controller. I found several posts stating that ST offers small companies to get a PID under the ST USB Vendor ID.Is this possible - how do we apply and what does it cost?We would like not to ...

EAlbr.1 by Associate
  • 5173 Views
  • 1 replies
  • 0 kudos

Resolved! LwIP echoclient RAW example comments

I wish this thread could be a community documentaiton to analyze and understand LwIP RAW echoclient example provided in firmware packages. It would be nice to open new threads for each example.First question regarding this example: in tcp_echoclient_...

JMarq.1 by Associate III
  • 2996 Views
  • 6 replies
  • 0 kudos

STM32F723 Problem USB with DMA in VCP Mode

Hello,I'm currently working on a project using the STM32F723 Discovery kit and USB as a Virtual Com Port (VCP) in CDC mode. I'm encountering an issue related to DMA and USB_OTG_HS when using the CubeMX configuration with the "Enable internal IP DMA" ...

CObri.1 by Associate III
  • 4282 Views
  • 6 replies
  • 0 kudos