2020-09-25 12:35 AM
bxCAN problem.
Now sending data from STM32F407 to STM32F042 via bxCAN.
In STM32F042, it is possible
and oscilloscope that having CAN analyzing could read the sending ID/data correctly.
But, STM32F042 is impossible to read the standard ID. The reading ID is 0x000.
What is my mistake ?
Sending ID is 0x555.
/* receive interrupt */
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan){
CAN_RxHeaderTypeDef RxHeader;
uint8_t RxData[2];
if(HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &RxHeader, RxData) == HAL_OK){
id = RxHeader.StdId;
dlc = RxHeader.DLC;
ide = RxHeader.IDE;
CANRxData[0] = RxData[0];
CANRxData[1] = RxData[1];
if(id == myID){
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_0); // Just a test
}
}
}
void CAN_Init(void){
CAN_FilterTypeDef filter;
filter.FilterIdHigh = 0;
filter.FilterIdLow = 0;
filter.FilterMaskIdHigh = 0;
filter.FilterMaskIdLow = 0;
filter.FilterScale = CAN_FILTERSCALE_32BIT;
filter.FilterFIFOAssignment = CAN_FILTER_FIFO0;
filter.FilterBank = 0;
filter.FilterMode = CAN_FILTERMODE_IDMASK;
filter.SlaveStartFilterBank = 14;
filter.FilterActivation = ENABLE;
HAL_CAN_ConfigFilter(&hcan, &filter);
}Tx side code is
void CANTx(void){
if(0 < HAL_CAN_GetTxMailboxesFreeLevel(&hcan1)){
CAN1TxHeader.StdId = 0x555;
CAN1TxHeader.RTR = CAN_RTR_DATA;
CAN1TxHeader.IDE = CAN_ID_STD;
CAN1TxHeader.DLC = 2;
CAN1TxHeader.TransmitGlobalTime = DISABLE;
CAN1TxData[0] = 0x11;
CAN1TxData[1] = 0x22;
HAL_CAN_AddTxMessage(&hcan1, &CAN1TxHeader, CAN1TxData, &CAN1TxMailbox);
}
}regards.
2022-05-10 12:22 PM
Today I got the same issue. After a lot of debugging with breakpoints I found the issue.
In the declaration of HAL_CAN_GetRxMessage in your ***.hal_can.c file you can see that the method want to have a data buffer of 8. If you are using less, the method overwrites your header data. So the simple fix for this issue was.
switch this line
uint8_t RxData[2];to this line
uint8_t RxData[8];