cancel
Showing results for 
Search instead for 
Did you mean: 

On L151, SPI Half duplex in pooling mode, HAL generate nb word length clock cycle more while reading

LROME.1
Associate

Hi FAEs and the community,

On a L151 the SPI block has a strange behavior.

Some time to time it generates 8 clock cycles more on a read (if I use size 8 bits) or 16 bits (if I use size 16 bits).

My target is a 16 bits based half duplex SPI device.

Thus it introduces a shift on the next read and messing up everything...

I use the HAL (HAL_SPI_Receive and HAL_SPI_Transmit).

Withe a prescaler at SPI_BAUDRATEPRESCALER_128 (means 250Khz) I have few errors.

If I go up to SPI_BAUDRATEPRESCALER_64 (in spec according the stm32l1xx_hal_spi.c file) then the error is immediate...

Does someone has seen this behavior before ? Is there a fix ?

Is there a way to flush the RX fifo datas (if any) from this IP (and I have a work around) ?

Thanks a lot

Regards

Lionel.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0