STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Implementing IWDG in sleep mode

I implemented IWDG  reset having counter of  12 second and am  refreshing it using HAL_IWDG_Refresh(&hiwdg) in while loop.  Everything is working as expected. But now the issue is when I implement sleep mode.  The processor will be in sleep and wakeu...

Nico3 by Senior
  • 4297 Views
  • 8 replies
  • 0 kudos

Self diagnostic feature

Dear All,I'm looking for self diagnostic feature in STM32F7 series for SIL-3 compatibility, kindly suggestion microcontroller which can self diagnosable crystal clock ,ECC protected sram and flash memory . and also let me know The HAL library is SIL-...

vchau.2 by Associate III
  • 2339 Views
  • 2 replies
  • 0 kudos

Resolved! Boot from external flash stm32h755

Hello, I am trying to boot from the external flash memory that the nucleo-h755zi-q has(addres->0x09000000), but I am having some issues. The idea I was following is :1. Create a Bootloader project, in this project I configure the QuapSPI in the inter...

Divide memory

Hello, I divided memory of the stm32h747. we want to divide memory in c code. there is below which ld file code we are using now. If there is better things than bellow, please give answerr.. MEMORY{RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512KFLA...

Snm.1 by Associate III
  • 907 Views
  • 0 replies
  • 0 kudos

adc_sampling

I have generated an pwm of 1khz from timer now I  want to read adc reading  for once for each cycle of pwm after 50 microsecond of rising edge how to do if anyone have code please send in stm 32 .

ishu by Associate II
  • 2194 Views
  • 3 replies
  • 0 kudos

COMPILATION WOLFSSL ERROR : unknown type name 'time_t'

Hi STCommunity,I have a project with X-CUBE-FREERTOS and it worked fine, since I added WolfSSL the build goes wrong because it doesn't seem to recognize "time_t". (registration file attached)I hope someone can help me. Many thanks in advance  

rdl by Associate III
  • 9880 Views
  • 8 replies
  • 0 kudos