AK.15
Associate II
since
2022-08-31
2023-06-14
User statistics
4
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About AK.15
Options
Report User
User Activity
Posts
Replies
Hello, I've tried to test sdcard with fatfs on STM32F429ZI on NUCLEO-F429ZI board. The same code was working in SD 1 bit mode((no DMA, no RTOS).when i configure SD 4 bit mode f_mount returns FR_NOT_READY.
2022-08-31
Re: Hello, I've tried to test sdcard with fatfs on STM32F429ZI on NUCLEO-F429ZI board. The same code was working in SD 1 bit mode((no DMA, no RTOS).when i configure SD 4 bit mode f_mount returns FR_NOT_READY.
2022-08-31
what are the possibility if the 4 bit mode not working?
Re: Hello, I've tried to test sdcard with fatfs on STM32F429ZI on NUCLEO-F429ZI board. The same code was working in SD 1 bit mode((no DMA, no RTOS).when i configure SD 4 bit mode f_mount returns FR_NOT_READY.
2022-08-31
Enable internally pull-ups on all lines except sdio _clk
Re: Hello, I've tried to test sdcard with fatfs on STM32F429ZI on NUCLEO-F429ZI board. The same code was working in SD 1 bit mode((no DMA, no RTOS).when i configure SD 4 bit mode f_mount returns FR_NOT_READY.
2022-08-31
I rechecked the wiring,it is okay.If any issue in my configuration,please check thatThe relevant part of code:fr = f_mount(&FatFs, "", 1); if(fr==FR_OK) { HAL_UART_Transmit(&huart3, "OK to mount\n\r", 15, 1000); } ...