STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Fx_NoR_Write_Read_File example for STM32U5x9J-DK

The example does not work. It times out:Stack:HAL_OSPI_AutoPolling() at stm32u5xx_hal_ospi.c:1,831 0x80042e8ospi_memory_reset() at lx_stm32_ospi_driver_glue.c:560 0x8001afelx_stm32_ospi_lowlevel_init() at lx_stm32_ospi_driver_glue.c:79 0x800165alx_st...

efekete by Associate
  • 2287 Views
  • 2 replies
  • 0 kudos

Resolved! Programming STM32H747AI

Hello,I am currently designing a board with STM32H747AI MCU. May I ask how it is possible to run the RTOS on it and then program it via USB-C without using special internal components such as ST-Link MCU in order to save as much space as possible? Do...

Implementing IWDG in sleep mode

I implemented IWDG  reset having counter of  12 second and am  refreshing it using HAL_IWDG_Refresh(&hiwdg) in while loop.  Everything is working as expected. But now the issue is when I implement sleep mode.  The processor will be in sleep and wakeu...

Nico3 by Senior
  • 4275 Views
  • 8 replies
  • 0 kudos

Self diagnostic feature

Dear All,I'm looking for self diagnostic feature in STM32F7 series for SIL-3 compatibility, kindly suggestion microcontroller which can self diagnosable crystal clock ,ECC protected sram and flash memory . and also let me know The HAL library is SIL-...

vchau.2 by Associate III
  • 2322 Views
  • 2 replies
  • 0 kudos

Resolved! Boot from external flash stm32h755

Hello, I am trying to boot from the external flash memory that the nucleo-h755zi-q has(addres->0x09000000), but I am having some issues. The idea I was following is :1. Create a Bootloader project, in this project I configure the QuapSPI in the inter...

Divide memory

Hello, I divided memory of the stm32h747. we want to divide memory in c code. there is below which ld file code we are using now. If there is better things than bellow, please give answerr.. MEMORY{RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512KFLA...

Snm.1 by Associate III
  • 903 Views
  • 0 replies
  • 0 kudos