STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB Type C DRD/OTG

hi all,  i am using STM32U585 controller which is having a internal UCPD controller.my requirement is to create a module which can act as host and device using USB type C. i am taking the hardware connection as same as stm32U585 eval board(and adding...

sabari1 by Associate III
  • 3785 Views
  • 1 replies
  • 0 kudos

Resolved! Bug in CRS register definition of STM32U585xx

Affected driver library: STM32Cube_FW_U5_V1.2.0File: stm32u585xx.hThe definition of CRS_CR_TRIM_Msk is wrong.Currently it is:#define CRS_CR_TRIM_Msk (0x3FUL << CRS_CR_TRIM_Pos) /*!< 0x00003F00 */But instead it should be:#define CRS_CR_TRIM_Msk (0x7FU...

SOfne.1 by Associate III
  • 1684 Views
  • 2 replies
  • 0 kudos

CORS with LWIP

Hi - can anyone tell me how to insert a CORS header into LWIP?(Cross-Origin Resource Sharing) header directly into the httpd.c? file of LwIP)i.e.Access-Control-Allow-Origin: *I am using vscode to debug an index.shtml file file, but i need to get resp...

Resolved! STM32L4S5VIT6 with AWS

Hi,    Good morning, everyone. I'm new to IOT. So, I need your help for how to connect and use STM32L4S5VIT6 and AWS from the scratch. Could you please help me. Demo video or any sample code and share any related document for understanding purpose it...

M_Sukumar by Associate III
  • 4983 Views
  • 10 replies
  • 0 kudos

Resolved! STM32H723 ADC Oversampling code generation bug

I am using STM32CubeIDE v1.13.2. When setting oversampling for ADC3 on STM32H723, the ratio value is incorrectly generated to exactly the number that is typed in the GUI:  hadc3.Init.Oversampling.Ratio = 32; which is then on lines 725-735 in stm32h7x...

heveskar_0-1697111110765.png

Resolved! PSSI_Transmit_Receive_DMA example does not work

Hello,I used two nucleo-H723ZG boards to try the PSSI_Transmit_Receive_DMA example code in the STM32Cube\Repository\STM32Cube_FW_H7_V1.11.1\Projects\NUCLEO-H723ZG\Examples\PSSI directory, the LEDs on both boards do not flash as expected (master board...