cancel
Showing results for 
Search instead for 
Did you mean: 

Problem writing to flash (STM32F051K6U6)

JFELI.13
Associate III

Hi

I'm using MikroC and try to play with Flash

My problem: even if area seem ok between "bootloader" and "program", I can see program area is not complete and is writed in bootloader area.

If you can help me ... thanks !

#pragma orgall 0xC0  /?
 
#define BOOTLOADER_START_ADDR  0xC0
 
#define START_PROGRAM_ADDR     0x1900  
 
#define FLASH_SIZE_STM32F051K6U6 16000 
 
#define FLASH_BACKUP_ADRESS ((FLASH_SIZE_STM32F051K6U6-START_PROGRAM_ADDR)/2)+0x1800
 
 
void main() org 0xC0 (bootloader) 
 
{
 
 char x1=0;
 
 SetIOs();
 
 Led_Red
 
 UART1_Init(9600);
 
 Delay_100ms();
 
 
 if(x1)FLASH_MOVE(START_PROGRAM_ADDR,FLASH_BACKUP_ADRESS,FAUX); /
 
 if (0) //UART1_Write_Loop('g','r'))
 
 {
 
     Start_Bootload(); // "r" recu -> start bootload
 
 }
 
 else
 
 {
 
     Start_Program();
 
 }
 
}
 
 
void program org 0x1900 (after boot control)
 
{
 
    uart1_write_Text("ESSAI");
 
}

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Javier1
Principal

what is microC, isnt that supposed to be for PICs?

hit me up in https://www.linkedin.com/in/javiermu%C3%B1oz/
MM..1
Chief III

Programming STM32 this way isnt good start. Ask on MicroC for ARM forums.

Or use STM32CubeIDE

JFELI.13
Associate III

MikroC exist for Pic & ARM (and some others)

I could use STM32Cube except it would need I modify many many files (I use MikroC from years) and I suppose it would take a long time to do so.

But could you explain me how to force routing positioning of the addressing in a compilation ?