Move/change default reset location of STM32F765
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-02-01 4:33 AM
We are trying to implement application which starts from location(eg. 0x0806 0000 of the flash) which other than default 0x0800 0000.
As per STM32F765 reference manual and AN2606 performed following steps,
- Switched to Dual bank mode of flash, nDBank = 0
- Enabled dual boot mode by nDBoot = 0
- nBoot0 pin is pulled low in the Hardware
- As nBoot0 pin is pulled low, Boot memory base address is defined by value hold by register BOOT_ADD0[15:0]
- Wanted to boot from flash at location 0x0806 0000. Hence putting value as 0x2018 into register BOOT_ADD0[15:0]. ( Value to be written in BOOT_ADD0[15:0] = Starting location(0x0806 0000) right shift by 14(divided by 16384)).
- In the linker file define symbol __ICFEDIT_intvec_start__ = 0x08060000
With above mentioned steps, when MCU is reset without running ST-Link, unable to execute code/unable to run application.
Am I missing any steps, could you help with this.
Thanks!
Labels:
- Labels:
-
Bootloader
-
STM32F7 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0