STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB_HS CONNECTION AND DICONNECTION CABLE

I AM USING IN USB_HS DEVICE MODE ,WHEN I CONNECT USB CABLE TO THE PC THEN I WANT  TO KNOWE WHERE IT IS DETECT AND AFTER THAT I REMOVE USB CABLE THEN WHRE IT IS DETECT GIVE ME ANY REGISTER OR CALL BACK FUNCTION ONLY TELL ME IN DEVICE MODE

SITARAM by Associate III
  • 2270 Views
  • 5 replies
  • 0 kudos

Resolved! Set Date&Time NUCLEO-401RE

Hello everyone, i am working on a software for setting the date and time. The plan is to set the date and tame manually (so no defficulties regarding that) and then continue to increase within the time flies thanks to the RTC of the NUCLEO F401RE.  D...

willow by Associate III
  • 2920 Views
  • 5 replies
  • 3 kudos

Resolved! STM32L562 EDK and USB PD

Hi Team,I have STM32L562 EDK with me , and can i make a USB PD application with that alone ?, or should i buy x-nucleo-snk1m1 which has TCPP01 for port protection?Expecting a quick replyThanks in advanceNithin

NITHIN by Associate III
  • 2493 Views
  • 4 replies
  • 5 kudos

Interfacing of stm32F446re with SD card

#include <stdio.h> #include <string.h> #include "fatfs.h" #include "fatfs_sd.h" #include "main.h" FATFS fs; FIL fil; FATFS* pfs; DWORD fre_clust; uint32_t totalSpace, freeSpace; /* Private includes -------------------------------------------------...

Premaa by Associate
  • 1719 Views
  • 2 replies
  • 0 kudos

Run USBX on STM32H563VIT

Sorry, Google Translate changed my previous post to Polish. That's probably why no one answered me.Now the post is correct. I'm creating a custom board using a used STM32H563VIT. Nice processor, but I can't understand how to create an Audo class, eve...

image.png image (1).png image (2).png image (3).png
konsul41 by Associate II
  • 7109 Views
  • 13 replies
  • 0 kudos

X-CUBE-CELLULAR for STM32H5

Hello,I am currently engaged in an IoT project utilizing the STM32H5 microcontroller unit (MCU). I would like to inquire whether the X-CUBE-CELLULAR library is available for the STM32H5 MCU. If it is not currently available, are there any plans to po...

Egemen by Associate II
  • 1371 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F767ZI: Hard fault with FreeRTOS mutexes + DMA I2C

My setting is a Nucleo F767ZI board with a IKS01A2 shield. I created a FreeRTOS project that periodically queries the temperature sensor, calculates an average of temperature data, and prints the temperature on the UART. It has three threads that wor...

PB1 by Associate III
  • 3331 Views
  • 5 replies
  • 5 kudos