Question
Nucleo F411 board is resetting when connect the USB ST_Link to computer.
Hi,
I have two Nucleo F411 board. When I connect the board to the computer with the USB ST_Link, one automatically reset and the other no. I don't want that the board automatically reset.
The HW configuration and program are exactly the same for the two board. The only change is that a board is a mb1136 c-04 (who reset) and the other is a mb1136 c-03 (who not reset).
I examine the two board but don't see any difference.
An idea to solve this problem ?
Thanks,
Lionel