STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32h743 library file for proteus

i need to add the stm32h743 in to the proteus , bcz i dont have the hardware.can anybody tell how to download stm32h743 library file for proteus  or  direct link to download file . thanks.....

OctoSPI configuration for hyperflash

does anyone have a configuration for the CypressS26KL256S hyperflash? in the stm32cube_fw_l4_v1130 are examples only for regular command mode (micron or macronix) but not for hyperflash mode. thanks in advance

Leo_Panda by Associate III
  • 7325 Views
  • 12 replies
  • 1 kudos

Stuck in application startup code

I am facing an issue on one of our stm32f4 boards. We have a custom bootloader , which boots up the app as below   __disable_irq(); HAL_RCC_DeInit(); __HAL_RCC_AHB1_FORCE_RESET(); __HAL_RCC_AHB1_RELEASE_RESET(); __HAL_RCC_AHB2_FORCE_RESET(); __HAL_...

krishr by Associate III
  • 2844 Views
  • 5 replies
  • 0 kudos

Resolved! building cloned project

Hi Team,I've recently cloned https://github.com/STMicroelectronics/STM32CubeL5/tree/master/Projects/STM32L562E-DK/Applications/USB-PD/USB-PD_Consumer_1port , for USB PD project.But when i imported the folder into workspace ,the build option is disabl...

NITHIN by Associate III
  • 4843 Views
  • 8 replies
  • 5 kudos

Resolved! when I build the project, it is showing the error of 1. .text' will not fit in region `FLASH' 2. `FLASH' overflowed by 12480 bytes

Hello everyone,I am working with stm32f070c6 , I am developing an application of USB_CDC , When I build the project it is showing the error of 1. .text' will not fit in region `FLASH'2. `FLASH' overflowed by 12480 bytesactually I had increase the hea...

RKUMA.2 by Associate II
  • 9045 Views
  • 6 replies
  • 0 kudos

Resolved! STM32F373 HAL functions for SDADC

Hello guys, I tried to use the HAL_SDAC functions to read two Analog signals (0-3.3V) with DMA but I didn't have good results.That's why I started reading only one Analog signal in Polling mode (ING 5)....unfortunately even in this case I always read...

Vero_0-1715778269997.png Vero_1-1715778306014.png
Vero by Associate III
  • 7528 Views
  • 10 replies
  • 0 kudos

Resolved! STM32F407 Ethernet MII Operation

I have custom hardware with a STMF407VET6 connecting to a ethernet switch via the MII interface.I am using STMCUBEIDE 1.15.1 to generate the basic code. For debugging I am using a barebones configuration for the ethernet connectivity and a GPIO to co...

GLCD only half screen is working

I am working on Graphic Display(JDH12864E) using STM32L031K6. I have written code and I found that my lcd is printing only half of screen.For example:- I try to print ("12345678912345") then it prints only ("123456789") it means it is printing only 1...