STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F303re SPI AT 18Mhz

Hello,I need assistance generating a continuous 18MHz SPI signal without gaps between data transmissions using the STM32F303RE. Additionally, I need to be able to perform other tasks on the microcontroller simultaneously.I am using DMA in circular mo...

mse by Associate II
  • 3177 Views
  • 6 replies
  • 0 kudos

STM32H723 SDMMC FIFO blocks while write data

I configured a FATFS project using STM32CUBEMX to write 248 bytes of data every 1ms, with a buffer accumulating up to 1024 bytes before writing to the SD card. However, I encountered significant blocking issues with f_write. To troubleshoot, I replac...

Blowind by Associate
  • 2722 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G4 DAC output HAL+LL naming

Hi,HAL and LL DAC configuration structure and its parameters naming can be confusing. Reference manual claims that DAC "mode" (register ADC->MCR, bits 0..2 or 16..17) can be in one of following four combinations when not used sample and hold mode: 0 ...

Error STSAFEA110 expansion board + X-NUCLEO-G474RE

Hi,Currently, I am testing the authentication example using STSAFEA110 expansion board with X-NUCLEO-G474RE.I follow the steps in STMicroelectronics.X-CUBE-SAFEA1_GettingStarted.pdf and also compared the STSAFEA110 expansion board+NUCLEO-L476RG Authe...

bay_2-1715244405871.png bay_1-1715244180085.png
bay by Associate II
  • 5123 Views
  • 5 replies
  • 0 kudos

Azure RTOS, FreeRTOS or SafeRTOS?

Hi all,I am writing to you to find out which is the best RTOS between Azure RTOS, FreeRTOS and SafeRTOS both from the point of view of performance and from the point of view of flexibility and ease of use?I have to develop some projects with STM32U5,...

Resolved! Problem with TIM3 Input capture with DMA

Hello everybody,I am trying to use the TIM3 those input capture mode with DMA transfer. After buffer is full the DMA call the callback function IT. Then i execute the stop DMA function. But after this sequence, the DMA no reinitialize. I am using the...

VSchu.1 by Associate II
  • 1958 Views
  • 4 replies
  • 0 kudos