STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB PD sink

Hi Team, I want to work on USB PD sink , which board would be suitable?, I'm trying for 28V 5A power. I think the firmware for this specification is not available yet. Even though i want to try on. Would you suggest me any board? Is STM32L562 would b...

NITHIN by Associate III
  • 4688 Views
  • 7 replies
  • 3 kudos

Resolved! FP-SNS-ALLMEMS1 not found in cube ide

HiI am trying to set up a project based on FP-SNS-ALLMEMS1.When i set up a project based on STM32L476 Nucleo, I cant find the pack neither under "select components" nor under "manage software packs". see belowWhy?? 

MK1_0-1717666159417.png
MK..1 by Senior
  • 1156 Views
  • 1 replies
  • 0 kudos

STM32G0 Unstable LSI frequency

Dear Everyone,We use STM32G0B0 MCU and in errata there's a section from the unstable LSI frequency. In some case the LSI frequency about 48 kHz. The workaround not work, after backup domain reset, the LSI frequency still about 48 kHz. My theory is th...

lwip_accept(..) getting blocked

I’ve created an STM32 project using STM32CubeIDE and enabled LWIP and FreeRTOS. My purpose is to run a basic TCP Server program on the STM3240G-Eval board using BSD sockets, containing two threads. I need to use most of the BSD socket calls such as l...

STM32F303re SPI AT 18Mhz

Hello,I need assistance generating a continuous 18MHz SPI signal without gaps between data transmissions using the STM32F303RE. Additionally, I need to be able to perform other tasks on the microcontroller simultaneously.I am using DMA in circular mo...

mse by Associate II
  • 3177 Views
  • 6 replies
  • 0 kudos