STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problem with TIM3 Input capture with DMA

Hello everybody,I am trying to use the TIM3 those input capture mode with DMA transfer. After buffer is full the DMA call the callback function IT. Then i execute the stop DMA function. But after this sequence, the DMA no reinitialize. I am using the...

VSchu.1 by Associate II
  • 1958 Views
  • 4 replies
  • 0 kudos

CAN Filter settings do not work properly.

void CAN_Filter(uint8_t filter_index, uint32_t Filter_ID){CanFilter.FilterType = FDCAN_FILTER_MASK;CanFilter.IdType = FDCAN_EXTENDED_ID;CanFilter.FilterIndex = filter_index;CanFilter.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;CanFilter.FilterID1 = Filter...

SJ_KIM by Associate
  • 2051 Views
  • 3 replies
  • 0 kudos

USB Host read gets interrupted

Hi y'all.I'm working on a project which uses a stm32 nucleo board (f446re) as both usb host and device, using USBFS as device and USBHS as host.The goal is to make some sort of interface between computer and memory sticks, which renders them as read ...

Using st firmware to control Vienna rectifer

I have used eDesignSuite to generate firmware code for my vienna rectifer. I need some more clarity/documentation on implementation of the code. Many things are unclear, such as at start-up, there is a pin dedicated to an relay, which will limit the ...

suyog800_0-1717043542115.png
suyog800 by Associate II
  • 1514 Views
  • 1 replies
  • 0 kudos

SMT32L4 CAN bootloader not initializing

I have a STM32L431 that jumps to the bootloader using a software jump to 0x1FFF0000.I verified that the PB8 and PB9 pins are used on my system and I also have a 8MHz crystal soldered. I let the bootloader run then I send a 0x79 standard identifier wi...

bareil76 by Associate II
  • 4299 Views
  • 2 replies
  • 0 kudos

Resolved! Custom HID Receive data

Hi,I'm using Custom HID class for sending MIDI messages by editing the descriptors. I am using sendReport function for sending MIDI messages, I want to receive MIDI messages as well. I was wondering whether there is any function to receive messages i...

kps98 by Associate III
  • 2120 Views
  • 2 replies
  • 1 kudos