cancel
Showing results for 
Search instead for 
Did you mean: 

declaring variables with ram address

madhavi U
Associate II

I declared some test variable like,

unsigned short *testvar= (unsigned short *)0x20020074;

unsigned char *testvar1[4] = {(unsigned char *)0x20020076,(unsigned char *)0x20020077,
                                                  (unsigned char *)0x20020078,(unsigned char*)0x20020079};

but unfortunately in mid I left some part of the ram space and again declared a variable like,

unsigned short *testvar2= (unsigned short *)0x20020092; 

I'm computing checksum from 0x20020074 to 0x20020092 and storing into flash , but  0x20020080 to 0x20020091 nowhere i'm declaring this space .is it create problem when i'm retrieving data from flash into ram?

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
FBL
ST Employee

Hello @madhavi U ,

 

Do you mean retrieving data from RAM to Flash?  you may need to check this post Solved: Declaring variables in SRAM1-3 areas of H7 devices... - STMicroelectronics Community

Hope this helps!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL