STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MDC / MDIO Read Write Failure

Hi All              I designed the hardware using the STM32H753VIT6 and the 3-port Ethernet switch KSZ9893RNXI. The STM32 is configured and can communicate with the external world via Ethernet. However, I'm unable to read or write to the switch regis...

HAL_GPIO_EXTI_IRQHandler Pin Or Port

I'm trying to wrap my head around HAL_GPIO_EXTI_IRQHandler...Why is only the "Pin" used in the parameter, and not the "Port". Really, why not both?According to en.DM00031020.pdf page 382 section 12.2.5 "External interrupt/event line mapping", it appe...

Resolved! USB HS on the STM32H7S3L8

Hello,I'm trying to use the USB-HS peripheral with the built-in PHY on Nucleo STM32H7S3L8I'm using CubeMX generated code from CubeIDE. I have not chosen the Nucleo board on CubeMX, because it was causing some issues with the MPU. Instead, I've chosen...

chintal_0-1730981775847.png
chintal by Associate II
  • 3358 Views
  • 4 replies
  • 6 kudos

Resolved! STM32G0x1 USB?

https://www.st.com/en/microcontrollers/stm32g0-series.html?icmp=tt9016_gl_****_dec2018&querycriteria=productId=SS1960 :but on https://www.st.com/content/st_com/en/products/microcontrollers/stm32-32-bit-arm-cortex-mcus/stm32-mainstream-mcus/stm32g0-se...

0690X000006CkQNQA0.png

Adding BSD sockets to netxDuo for LLDP

Hi,I was able to run a demo project on a STM32H573 dev board. I am using ThreadX and NetxDuo, with mqtt addon.I was able to connect to the mqtt broker and send/receive messages.I want also to be able to use the bsd sockets to send packets on layer 2....

coso2 by Associate II
  • 2647 Views
  • 4 replies
  • 2 kudos