STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[Synopsys OTG] FIFO clash

So where exactly does the documentation say that different FIFOs can't be accessed simultaneously?In dervice mode, an In endpoint was configured to transmit one 16-byte-long packet, and then 16 bytes (i.e. 4 words, 72 43 70 A4 D9 99 55 2E 19 7F 32 37...

0690X000006C5xoQAC.png

Resolved! No Example QSPI SDK for STM32F413H

Hi i am using Nucleo - F413ZH i need to work on the QSPI protocol i found this device supports QSPI but in the repository i doesn't find any example code for this one is this device supports QSPI? or is there any similar sdk so that we can import pro...

avinpat_8_0-1742817721795.png
avinpat_8 by Associate III
  • 2080 Views
  • 6 replies
  • 0 kudos

Resolved! DPM_Sleep_start build error

Hi Pascal, We have designed a custom PCB, and I’m attaching the schematic for your reference. Since we don’t have a dedicated UART, we have not enabled trace embedding. We are using X-CUBE FreeRTOS 1.3 with STM32U575VGT6. The USB dual-role functional...

ucpd_schimatic1.png ucpd_schimatic.png ucpd_error.PNG

Mbedtls porting in STM32L462REY6TR

Hi,I am having a lot of issues trying to port MbedTLS in my board B-l462e CELL1. I am trying to use the cellular project from X-Cube-Cellular and integrate MbedTLS to be able to connect to AWS. I can't find it in the CubeMX so I figured I need to por...

SSWM by Associate III
  • 1737 Views
  • 2 replies
  • 0 kudos